Hello,
I am using CCS5.2.1.000.18 with the C6746. When I want to do a system reset (ctrl+shift+S) somehow my processor crashes and I get the following message:
Trouble Halting Target CPU:
Error 0x00001020/-1137
Error during: Execution, Target,
It appears that the target is being held in reset. This may be
due to Wait-In-Reset (WIR) configuration set by the EMU 0/1 pin
settings. If this is the case, press Cancel and disconnect all
connected devices to attempt to clear the WIR configuration.
If this is a multi-core system, the master CPU or ICEPick may
not be releasing the target from reset. Please check your
configuration and/or your GEL files to ensure that nothing
is blocking the target from being released from reset.
it is impossible at this point to recover unless I do a complete power down then up of my board. I am attaching my .gel file just in case.
I appreciate the help,
thx.1882.C6746.gel