I am trying to install my floating license for CCS v5 on a server that I have been successfully using for other FlexLM licenses, but when I check the staus of the server, there is a Winsock error that is preventing the tidspssw daemon from working. The results of a status enquiry from lmtools is copied below. from a Can anyone help?
--------
Status
--------
Flexible License Manager status on Fri 8/3/2012 16:14
[Detecting lmgrd processes...]
License server status: 27000@uspl-print2
License file(s) on uspl-print2: C:\Altera_License_Server\TMDSCCS-ALLF05-v5.lic:
uspl-print2: license server UP (MASTER) v11.10
Vendor daemon status (on uspl-print2):
tidspssw: Cannot connect to license server system.
The license server manager (lmgrd) has not been started yet,
the wrong port@host or license file is being used, or the
port or hostname in the license file has been changed.
Server name: 192.62.143.144
License path: 27000@uspl-print2;
FLEXnet Licensing error:-15,10. System Error: 10049 "WinSock: Invalid address"
For further information, refer to the FLEXnet Licensing documentation,
available at "www.flexerasoftware.com".