Being very new to CCS & recently tested Keil on this same package 9017, within minutes was building the project without much effort. That's not the case with CCS V5.2.1 simply importing an existing Ti built Eclipse project is being very difficult. Would simply like to open the original CCS folder project but No option to open an existing project so the import wizard has to TRY and make sense of the Includes paths.
The problem after importing and deleting this same project 20 times with only 1 successful compile - compiler started to complain about Symbols not being found on successive runs so how it actually created a 49k bin file build the exact size of the packed bin is beyond my imagination to figure out.
This is what I have figured out so far ; CCS does not generate the proper include path names when the import source files path are source file folders in the CCS work spaces directory. It was necessary to remove the default includes path syntax under C/C++ General Paths & Symbols properties in order to clear the path warnings to even get this far.
I'd like to see the tree of all project source files that came in the Ti package source imported to the solution, while importing from any other directory not being the WSD only copies over a few of the files from the discovered Ti CCS selected projects while it leaves the include source files in their home folder and creating an original project root path entry in the linked resources variables properties dialog. This was the only solution that actually would build the project one time while any repeat builds failed stating "Error ## Symbols not found" escalating the error ## count of Symbols missing up and down every successive build or rebuild. Checked the permissions on WSD folders each show ownership all folders below root.
In this example below the project source files were homed in the WSD path prior to importing - then setting Linked resources path variable of original project root to the new target folders under the WSD.