This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error compiling and loading program to launchpad.



 Hi friends,

this is my first try given to launchpad 

I installed the ccs compiler yesterday and since then, i am trying to compile the blink your LED program given in TI wiki. 

When I press the debug button, I get the error in a window stating,

 

"Load program error

Encountered a problem loading file:

C:\Users\thinkanish\LPad_workspace\Blink_LED\Debug\Blink_LED.out

Could not open file"

and in the output console, I get,

"MSP430: GEL: Encountered a problem Loading file: C:\Users\thinkanish\LPad_workspace\Blink_LED\Debug\Blink_LED.out  Could not open file"

Thanks. 

  • Hi Anish,

    what OS are you on?  Do you have full permissions?  It looks like the path got doubled somehow

    C:\Users\thinkanish\LPad_workspace\Blink_LED\Debug\Blink_LED.out

    Can you verify where the .out is located?  Can you try manually loading it?  Go to the debug perspecitve and try Run->Load->Load Program

    Any further details on what you are experiencing and attempting would help as well.  Please keep us informed.

    Best Regards,

    Lisa

  •  Hi Lisa,

    Thankyou for your reply.

    I am running windows 7 professional. 

    Yeah I have full permission as I am only admin user account in my laptop. Also, i am using the latest version of ccs 

    I dont know where the .out is located.! but I think that it is not created itself! When i Build the project,

    The output of the console is this:


    **** Build of configuration Debug for project Blink_LED ****

    C:\ti\ccsv5\utils\bin\gmake -k all
    gmake: *** [main.obj] Error 1
    gmake: Target `all' not remade because of errors.

    **** Build Finished ****

    Kindly help.

  • Hi Anish,

    I need details on how you imported the project/what you are attempting, what errors you see etc etc.

    Best Regards,

    Lisa

  • Hi Lisa,

    Sorry, the fault was mine!

    And Comodo internet security that i use.. It constantly sandboxed the .out file

    Disabling the antivirus and firewall did the job.

    Thanks for your time :) 

  • HI Anish,

    ok, glad to hear things got sorted.  All the best with development

    Best Regards,

    Lisa

  • I also got the same problem

    CortexR4: GEL: Encountered a problem loading file: C:\Users\K.Manjunathan\workspace_v6_0\fool\Debug\fool.out Could not open file

    How to rectify this problem

    Regards

    K.Manjunathan

    PSGIAS.

  • i tried manually but the problem is Load program option is not enabled in debug perspective