This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

please give me a new and full xds100v3 2.0 package,and i find the web download have not the dtsa_a3p060.stp

thanks a lot,i make a xds100v3 use a3p060,but i find the xds100v3 wiki's download files have not the V2.0 dtsa_a3p060.STP,and the xds100v3 1.0 can not work ,please help me.and my email:

lzgjxh@163.com 

 or lzgjxh@hotmail.com

tnanks a lot

 

  • Hi,

    The project <v3_fpga_2.prj> in the FPGA directory of the Rev 2.0 Design Kit should allow you to create the FPGA image for the a3p060, did you try that?

    In any case, I was able to dig the FPGA image <dtsa_a3p060.stp> file from a previous version of the software package and send it attached. Please use it at your own risk, as I am not sure if any changes were introduced in the Rev 2.0 Design Kit that required this file to be removed from the package.

    Regards,

    Rafael

    dtsa_a3p060.zip
  •  hello  ,thanks,and this file with xds100v2 1.0,but it can not work ,i have tested.

    and i have Re-Synthesizing the v3_fpga_2,and it have error,it can not Re-Synthesizing,so i want you can give me a you have tested xds100v3 2.0 file with full and Re-Synthesizing   v3_fpga_2,or you give a useable dtsa_a3p060.stp,and i can use xds100v3.thanks a lot.

  • and i use a3p125.stp and a3p125 is ok,but a3p125 can not use in my design,so i need a3p060 do xds100v3 2.0

    and i use you give me 060.stp,it can not work,the error is

    Error connecting to the target:
    (Error -180 @ 0x0)
    The controller has detected a target power loss.
    The user must turn-on or connect the power supply for the target.
    (Emulation package 5.0.747.0)

    and test

    [Start]

    Execute the command:

    %ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

    [Result]


    -----[Print the board config pathname(s)]------------------------------------

    C:\DOCUME~1\ADMINI~1\LOCALS~1\APPLIC~1\.TI\
        213602635\0\0\BrdDat\testBoard.dat

    -----[Print the reset-command software log-file]-----------------------------

    This utility has selected a 100- or 510-class product.
    This utility will load the adapter 'jioserdesusbv3.dll'.
    The library build date was 'May 30 2012'.
    The library build time was '22:52:27'.
    The library package version is '5.0.747.0'.
    The library component version is '35.34.40.0'.
    The controller does not use a programmable FPGA.

    An error occurred while hard opening the controller.

    -----[An error has occurred and this utility has aborted]--------------------

    This error is generated by TI's USCIF driver or utilities.

    The value is '-180' (0xffffff4c).
    The title is 'SC_ERR_CTL_NO_TRG_POWER'.

    The explanation is:
    The controller has detected a target power loss.
    The user must turn-on or connect the power supply for the target.

    [End]

    and i have  turn-on or connect the power supply for the target. serveral times.

    thanks a lot.please give me a useful dtsa_a3p060.stp with xds100v3 2.0

  • Hi,

    Thanks to the great work from one of our developers, please check attached a synthesized image of the Rev 2.0 design for the A3P060 FPGA.

    I am not sure if this is the only missing piece that will solve all the target power detection issues you are having, but at least you know this is the latest rev.

    The comments from the developer:

    There really isn’t any reason the A3P060 FPGA cannot be used, I guess when we did the update, we forgot to update that flavor FPGA as well.  We were having issues with the on chip PLL where it wouldn’t run reliably, so we had to re-design the XDS100v3 with a 100 Mhz clock instead of a 2 MHZ clock.

    Please give this a try and let me know the results.

    Regards,

    Rafael

    dtsa_a3p060.zip
  • Very grateful to the TI series emulator for the launch of the low-end users XDS100V3 after my test burning documents can you help me solve a big problem, because the mass production of a number of XDS100V3 its isolation Editionthe emulator can suddenly buy on the market A3P125 unavailable, still looking for why, but it takes time. If you can FPGA project XDS100V3, the latest sent me a copy of the possibility, I want to re-compiled, thank you. finally, I do so XDS100V3

    http://item.taobao.com/item.htm?spm=a1z10.1.11-17459868654.23.QguNX5&id=16423921653

    http://www.aliexpress.com/store/product/XDS100V3-TI-DSP-ARM-emulator-starting-at-home-the-size-of-a-business-card-the-higher/715836_683148916.html

     

    Thank you for helping me to solve this problem