This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Code Composer Studio V5. Linux devlopment AM335x.

We have just purchased this software packet, but I am very confused what this software offers.

Both CCS and ti-sdk-am335x-evm-05.06.00.00-linux-x86-install is installed under Ububtu 12.04 LTE.

I can compile the Linux target, but now my problems starts.

I did not expect that the Linux kernel could be compiled under windows.

I did expect that the CCS could compile my Linux Application under Windows. I did ask Arrow in denmark, whether this was possible and they did reply positive.

But I cannot see how to setup the environment under windows, and did also expect that the CCS did setup all relevant settings for crosscompiling etc.

I have same problem with CCS under Unbuntu, unless CCS only can run with MakeFiles, which complicates the process.

If I compare CCS with the eclipse environment from DIGI, which handles all Linux modules inside the Eclipse, then the benefits I get from CCS are every low.

Maybe I am doing something wrong.

 

Best Regards

Søren Svanemose