This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS 5.4 Texas Instruments XDS100v1 USB Emulator/C28xx : Target must be connected before loading program.

Hi,

I can run/load my Program into the RAm or into the Flash and I had no problems with it until CCS 5.3 and CCS 5.4.

Since this versions, everytime I want to Debug the Program an load it into the Flash, the error written in the Subject occures. I always have to connect with "right click -> connect to target" and then download with "Run -> Load ->....".

Why is it not funktion anymore automatic?