Hello,
I have enabled in Project properties->Build->Nehaviour->Enable parallel build->Use number of processors(4) and it was building using all 4 cores just fine, CPU was 100%, but 2 days ago I've added in pre-build step a command to call an executable and since then it builds only on one core, processor load is 25% and is 3 times slower. I tried removing the pre-build step, deleting workspace and is doing the same. I can see the gmake command is "gmake -k -j 4 all".
Any idea what happened?
Z:\>echo %NUMBER_OF_PROCESSORS%
4
Best regards,
David.