I am able to blink the lights using CSS 4.2.4 and also allowed to listen to music using other usb port but when I import the led project from css 4.2.4 using existing code composer studio in css 5 I am allowed to import the project and i test the target and it works ok but when i go and build the led project i get the following error.
*** Clean-only build of configuration Debug for project led ****
"C:\\ti\\ccsv5\\utils\\bin\\gmake" -k clean
DEL /F "led.out"
Could Not Find C:\Texas Instruments\ccsv4\emulation\boards\ezdsp5535_v1\tests\led\Debug\led.out
DEL /F ".\led_test.obj" ".\main.obj"
Could Not Find C:\Texas Instruments\ccsv4\emulation\boards\ezdsp5535_v1\tests\led\Debug\led_test.obj
DEL /F ".\led_test.pp" ".\main.pp"
Could Not Find C:\Texas Instruments\ccsv4\emulation\boards\ezdsp5535_v1\tests\led\Debug\led_test.pp
' '
**** Build Finished ****
Buildfile generation error occurred..
Build-configuration 'Debug' does not exist in the referenced project 'ezdsp5535bsl'. Use the 'Properties > Build > Dependencies' page to select an existing build-configuration.
Build stopped..
If you could provide some insight I really like to use ccs5 to use my 320 development platform
thanks in advance
regards,
Jeff