This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6713 Linker-generated copy tables different CCS3.3 vs. CCS5.5

All:

I posted this on the C6000 forum, but it may be better posted here.

http://e2e.ti.com/support/dsp/tms320c6000_high_performance_dsps/f/115/t/302894.aspx

 

C6713B

DSP/BIOS 5.41

CGT 7.03 on CCS3.3,

CGT 7.46 (or 7.03) on CCS5.5

Custom Target with 6713 IRAM, external SBSRAM, external Flash.

 

 

  • Todd,

    I moved your original post to the compiler forum.

    Thanks

    ki

  • I found a way to fix the problem - by importing from CCS 3.3, I was able to get a basic project with errors that needed correcting. The biggest correction was to go into the linked bios file and comment out only the MEMORY and associated defines. I have then been able to get a project with no errors and 165 warnings...but it did give me a hex file that I could load into our target system and see a successful outcome.