Other Parts Discussed in Thread: TMS320DM6435
When I am trying to connect the Blackhawk USB560V2 system trace emulator to DM6435 I got the follow error:
"IcePick_C_0: Error connecting to the target: (Error -1265 @ 0x0) Device ID is not recognized or is not supported by driver. Confirm device and emulator configuration is correct, or update device driver. (Emulation package 5.1.402.0)"
CCS version 5.5.0.00077.
Target Configuration setting:
Connection: Blackhawk XDS560v2-USB System Trace Emulator
Board or Device: TMS320DM6435
DM6435 is in the devices list that USB560V2 supports.
Any idea what could be the problem?
Regards,
GanZ