Other Parts Discussed in Thread: TM4C123GH6PM
Attempts to use a Tiva Launchpad with CCSv6 beta 4 running on CentOS 6.5 fails with the following error reported in the CCS console when attempt to start a debug session:
The same error has been seen on a CentOS 6.5 32-bit and CentOS 6.5 64-bit installation.CORTEX_M4_0: GEL Output:
Memory Map Initialization Complete
CORTEX_M4_0: Error connecting to the target: Frequency is out of range.
The Tiva Launchpad works OK with CCSv6 beta 4 running on Windows XP, so suspect a problem with the CCS Linux setup.