This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ccs_setup_6.0.0.00175.bin silently exits on CentOS 6.5 64-bit if glibc.i686 or libX11.i686 not installed

Tried to run ccs_setup_6.0.0.00175.bin on a fresh CentOS 6.5 64-bit installation, and it just silently exited without reporting any errors.

There were two problem with missing dependencies:

1) /lib/ld-linux.so.2 was missing, which caused ccs_setup_6.0.0.00175.bin to exit immediately without reporting any errors. Installing libc.i686 resolved this dependency.

2) libX11.so.6 was missing, which caused ccs_setup_6.0.0.00175.bin to exit after several seconds without reporting any errors. Installing libX11.i686 resolved this dependency.


Running ccs_setup_6.0.0.00175.bin then reported other 32-bit system libraries which were missing [as expected since was installing on a 64-bit OS]

Was it intended that ccs_setup_6.0.0.00175.bin should be able to report an informative message if  /lib/ld-linux.so.2 or libX11.so.6 can't be found?