This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Trace Viewer Columns Rearrange themselves again on enable/disable of other columns

This is just a minor point but it's annoying so wondering if there is a way to change the behavior.

I prefer to see the trace viewer organized with the program address, then the code, then the disassembly, then the source, and then stuff like read/write addresses for data trace and cycle counts.

This means when I start the trace viewer the first time, I have to do some re-arranging of columns.  It's not bad but it takes a little time and the screen refreshes / blinks a bunch of times which isn't very comfortable to look at.

Ok so once is fine, but what I'm finding is that if I turn on or off certain columns (like let's say I want to hide the cycle count to fit the rest of the info better on the screen) then it puts all the columns back to the original order at the same time I hide/show this one column.  So it makes me repeat the whole process of adjusting the column order again.

Would like it to be more like Excel where hiding / showing a column doesn't re-arrange the order of the other columns in the table (or their widths...)

Is that possible?