This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XDS200 - attempt to access the named emulator via USCIF ECOM has failed.



I'm having an issue with my Spectrum Digital XDS200 debugger. I haven't used in a few months, and now when I try to test the connection in target config I get the following message:

[Start]

Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\Paul\AppData\Local\.TI\1989394224\
    0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 560/2xx-class product.
This utility will load the program 'xds2xxu.out'.
E_RPCENV_IO_ERROR(-6) No connection
Failed to open i/o connection (xds2xxu:0)

An error occurred while soft opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.

The explanation is:
An attempt to access the named emulator via USCIF ECOM has failed.

[End]

The XDS200 shows up in Device Manager as two CDC serial ports, one Emulator and one User. I've tried to uninstall the drivers and so on without success.

Any suggestions on what I should try next?

Thanks in advance,

Paul.