This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

JTAG on OMAP5432



Hello,

I'm trying to get the JTAG working on the OMAP5432 to be able to test the DDRs that are connected. I have the basic part of the JTAG working, ie: IDcode, Instruction capture, boundary registry length & bypass.

When extest instruction is selected for interconnect testing, most of the pins on the DDRs are stuck low. I'm trying to drive the CS (chip select) high to disable the DDRs and even that pin is stuck low. Any ideas?? My JTAG tool is ASSET. Is there a compliance pin thats not mentioned in the bsdl file?

Thanks,

Brian

  • Hello  Brian.

    Did you solve this problema??

    I have the same problem. 

    Also silicon nails test for DDR fails in output pins, CLK, CS, Data, etc... reads "0", expect "1".

     

    working on X1149

    Regards.

    ps:

    ----------------------------

    -- OMAP5432 ES2 BSDL

    -- F791717                         

    -- V0.94

    -- April 23rd 2013

    ----------------------------

    entity F791717 is

       generic(PHYSICAL_PIN_MAP : string := "F791717_package");

  • did you sove this problem?

    same issue on x1149 tool