Other Parts Discussed in Thread: DAC5686
In this thread: http://e2e.ti.com/support/data_converters/high_speed_data_converters/f/68/p/374137/1317502#1317502 Ken had a very cool idea about setting up DAC5682 to generate some output by setting it in offset binary mode and using CMI1 to Fs/4 and setting the data input to the DAC to 0.
We have all the data line to the DAC to 0 and SYNC high but our output is not quite sinusoidal and the frequency of the output is ~26MHz like you can see bellow. All the registers are the default values with the exception of register 0x2 which is 0x48.
CLKIN is 40MHz and DCLK is 20MHz. What could be the issue?
Thanks,
Valentin