I have followed all instructions, tried on more than one machine, regardless of what I do I always end up with problems with the vendor daemon unable to start. See attached Log file. I have changed hosts, used lmtools to configure, used web gui to configure, I’m ensured that the exe files are not blocked. My firewall is not running on the server.
Both .lic file and tidspssw.exe (and.exe.manifest) are in the same folder as lmgrd.exe. I have downloaded all software from links on the guide here: http://processors.wiki.ti.com/index.php/License_Server_Administration_for_CCS
OS I have tried are Windows server 2003 R2 and windows server and windows server 2003 R2 64bit. Both come back with the same error. I have installed the required C++ redist as suggested. I've also restarted the host machines to see if that helped to no avail.
Extract from log file for latest attempt using lmtools to config service:
12:38:58 (lmgrd)
12:38:58 (lmgrd) Server's System Date and Time: Wed May 20 2015 12:38:58 GMT Daylight Time
12:38:58 (lmgrd) pid 4192
12:38:58 (lmgrd) SLOG: Summary LOG statistics is enabled.
12:38:58 (lmgrd) Detecting other license server manager (lmgrd) processes...
12:38:58 (lmgrd) Done rereading
12:38:58 (lmgrd) FlexNet Licensing (v11.12.1.1 build 150159 i86_n3) started on AGDMSPA01 (IBM PC) (5/20/2015)
12:38:58 (lmgrd) Copyright (c) 1988-2014 Flexera Software LLC. All Rights Reserved.
12:38:58 (lmgrd) World Wide Web: http://www.flexerasoftware.com
12:38:58 (lmgrd) License file(s): C:\Program Files\FlexNet Publisher License Server Manager\TMDSCCS-ALLF01-v6.lic
12:38:58 (lmgrd) lmgrd tcp-port 27001
12:38:58 (lmgrd) (@lmgrd-SLOG@) ===============================================
12:38:58 (lmgrd) (@lmgrd-SLOG@) === LMGRD ===
12:38:58 (lmgrd) (@lmgrd-SLOG@) Start-Date: Wed May 20 2015 12:38:58 GMT Daylight Time
12:38:58 (lmgrd) (@lmgrd-SLOG@) PID: 4192
12:38:58 (lmgrd) (@lmgrd-SLOG@) LMGRD Version: v11.12.1.1 build 150159 i86_n3 ( build 150159 (ipv6))
12:38:58 (lmgrd) (@lmgrd-SLOG@)
12:38:58 (lmgrd) (@lmgrd-SLOG@) === Network Info ===
12:38:58 (lmgrd) (@lmgrd-SLOG@) Socket interface: IPV4
12:38:58 (lmgrd) (@lmgrd-SLOG@) Listening port: 27001
12:38:58 (lmgrd) (@lmgrd-SLOG@)
12:38:58 (lmgrd) (@lmgrd-SLOG@) === Startup Info ===
12:38:58 (lmgrd) (@lmgrd-SLOG@) Is LS run as a service: Yes
12:38:58 (lmgrd) (@lmgrd-SLOG@) Server Configuration: Single Server
12:38:58 (lmgrd) (@lmgrd-SLOG@) Command-line options used at LS startup: -c C:\Program Files\FlexNet Publisher License Server Manager\TMDSCCS-ALLF01-v6.lic -l C:\Program Files\FlexNet Publisher License Server Manager\debug.log -z -s
12:38:58 (lmgrd) (@lmgrd-SLOG@) License file(s) used: C:\Program Files\FlexNet Publisher License Server Manager\TMDSCCS-ALLF01-v6.lic
12:38:58 (lmgrd) (@lmgrd-SLOG@) ===============================================
12:38:58 (lmgrd) Starting vendor daemons ...
12:38:58 (lmgrd) License server manager (lmgrd) startup failed:
12:38:58 (lmgrd) CreateProcess error code: 0xc1 File= tidspssw.exe