This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Makefile for CCS project

Hi , 

Is it possible to build a CCS project using an external makefile ?

As of now CCS automatically generates the makefile using the " ${CCS_UTILS_DIR}/bin/gmake -k " command .

Scenario : Based on the configuration file i want to include and exclude certain header directories in the project . For this purpose i wrote a makefile script but was not able to figure out a way to make CCS  build using that.

Is there any way of gmake command to build using external cmakefile.

I have searched Wiki & forum and could not find any useful pointers to the issue .  

CCS Version : 5.5

OS : Windows 7 - 64 bit

Compiler version : c6000_7.4.4

gmake application version : 3.81 

regards , 

vinodh