I got a debug error on my "main machine" running a licensed copy of CCSv6.1.0, so
I did a clean install of CCSv6.1.1 on another machine, choosing install options for
MSP430, MSP432, and TivaC. I accepting all the defaults and created a workspace in
D:\TI\MSP432_WS\. I ran CCSv6.1.1 and used App Center to install/update the
following CCS Add-ons:
MSP430 GCC MSPWare GUI Composer CC3200 Add-On
TI-RTOS for MSP43x TI-RTOS for TivaC TI-RTOS for Simplet.. TI ARM Compiler
MSP430 Compiler Javascript Develop.. CDT GNU ARM GCC
Grace Peripheral Co..
I used TI Resource Explorer to import the project:
C:\ti\msp430\MSPWare_2_30_00_49\driverlib\examples\MSP432P4xx\uart\uart_loopback_48mhz_brclk
I connected a MSP432P401R LaunchPad, compiled, and ran the program, which echoed
characters to Tera Term at 115,200 baud (as expected). When I paused operation to
look at variables with the Debugger, I got the following error:
Can't find a source file at "C:\space\msp432-driverlib\build\MSP432P4xx/cpu.c"
Locate the file or edit the source lookup path to include its location.
This is the exact same error that I had gotten on the other PC running CCSv6.1.0.
I could resume the program operation and it appeared to operate properly, but I
could not pause and look at variables with the debugger.
Can anyone give me a hand? Where do I find "source lookup path"?
Thanks,
Jim Smith