Making use of the CCS cloud on mac osx and on linux, the msp432 xds110 firmware was upgraded to the 2.2.4.2 version. Afterwards, I have tried to use it with CCS, and it was imposible to connect with the debugger. I tried to downgrade it to 2.2.4.0 using the firmware.bin available in the CCS, but it stills stays in 2.2.4.2.
Is there a solution to downgrade the firmware, or upgrade the CCS driver?
Thanks in advance,
Jose M.