This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DWARF information is corrupted



Hi

I have a very large out file (~385MB)

To the target i load the out file without symbols.

When i try to load the symbols I get Dwarf Information is corrupted.

I turned on the log file and found out this printed

0x0001C354 23839 4 OFS E: Paged file: failed to map region file=myoutfile.out offset=6408688 size=143207117 what=Not enough storage is available to process this command.

0x0001C354 23839 4 OFS_DWARF D: Processing compilation unit. Buffer is at 00000000, 0x8892acd long, starting at 0x0
0x00019EA0 23839 3 COM_DBG_IF C: class DebugEngine_Progress_Stream::OnUpdate()

Usually closing the code composer and opening it again, will fix it.

Is there any way to fix it for good?

I am using code composer 6

Thanks

Shiran