Hi,
I migrated weeks ago a project to the CCSv6.0.1 and then to CCSv6.1.1 it all worked fine until yesterday. Now I constantly get the following error:
Console Output:
"C:\\ti\\ccsv6.1.1\\ccsv6\\utils\\bin\\gmake" -k all
gmake: *** No rule to make target `D:/projects/THDA/Firmware/GIT_repo_complete/Firmware/trunk/Debug - Kopie/configPkg/config.bld', needed by `configPkg/linker.cmd'.
gmake: Target `all' not remade because of errors.
1. The folder >Debug - Kopie< does not even exist anymore! --> why is it mentioned and how can it be deleted?
2. setup a new Project didn't change anything
3. I tried to add the --clean option to the CCS exe file. --> no change
4. In CCS6.1.1 the Errors displayed in the Problems Tab are deleted when you change to this tab. So normally the Console output is simply >not remade because of errors< how should it be possible to work with such a tool?
5. trying to open the project again in CCS6.0.1 is not possible because the import is canceled with the error message that the compiler 6.4.x is not installed. So it can't import... (why is the import different if the compiler version in the project is higher than the current installation? --> why isn't it possible to select another compiler when the project is opened.
6. and most important, why is there now an automatic linker file generation? it always worked fine to have a linker cmd file in the project, now the automatic generated file generates problems with the cmd file in the project how can this be turned off?