Other Parts Discussed in Thread: AM1802
I saw in this thread that there were some recommendations to get past errors in the update, but in my case, I get no errors. But my swRev value stays at 1.0.0.2.
When I start CCS 6.1 and Launch my Target Configuration for the EVMK2X, it warns me that the firmware needs to be updated. I can Ignore that and am able to do all the emulation and work that I need to do, but I would like to get the update done successfully.
Using a Cmd window in Windows 7, I cd to the folder C:\TI\CCSv6.1\ccsv6\ccs_base\common\uscif\xds2xx which does have the 1.0.0.6 files as needed for the update. I then run the update bat file, but it shows that I have not actually been updated:
You can see that it seems to run, no errors, but fails to change the swRev value.
This is a very old EVMK2X from the early batch of the EVMs, but I would expect it to work in terms of the emulator.
My laptop only have USB 3.0 ports. It was recommended to the user at the earlier thread I referenced that he should try a USB 2.0 port. Would it or should it help if I hooked up through a USB 2.0 hub, or would that just make it worse? Or should I go try another computer with just the files in this xds2xx folder (not the rest of CCS installed, like my home PC)?
Device manager shows the two ports being there, and they are low numbers, COM5 and COM3 for the Emulator and User CDC ports, resp.
Thanks for any advice.
Regards,
RandyP