Other Parts Discussed in Thread: CC3200
This is weird. It seems that output sent to stderr is printed at a rate of 1 char per second, while output sent to stdout is fine.
I took the "blinky" example and added the following code to main.c:
GPIO_IF_LedOff(MCU_ALL_LED_IND);
setvbuf(stdout, NULL, _IOLBF, 0);
setvbuf(stderr, NULL, _IOLBF, 0);
printf("Hello, world!\n");
fprintf(stderr, "Error\n");
fprintf(stdout, "Done\n");
//
// Start the LEDBlinkyRoutine
//
i'm setting both stdout to line buffered mode, the print strings to stdout, then stderr, then stdout again (using fprintf this time, but it doesn't matter).
The result is: "Hello world appears instantly", then i get E-r-r-o-r-\n printed one char at a time, with approximately 1 second between each, then "Done" is printed instantly and the code continues on to blink the LEDs.
I'm using CCS 6.1.2.00015 on Ubuntu 15.10
Here, i even shot a video: https://youtu.be/R1Am9HSkQuw