Hello forum,
I am new to RTOS and I am trying to load the GPIO interrupt example on a EK-TM4C1294XL LaunchPad. But I am having a hard time building this example. When I do so the following errors appear in the console:
**** Build of configuration Debug for project gpiointerrupt_EK_TM4C1294XL_TI_TivaTM4C1294NCPDT ****
"C:\\ti\\ccsv6\\utils\\bin\\gmake" -k all
'Building file: ../gpiointerrupt.cfg'
'Invoking: XDCtools'
"C:/ti/xdctools_3_31_01_33_core/xs" --xdcpath="C:/ti/tirtos_tivac_2_14_04_31/packages;C:/ti/tirtos_tivac_2_14_04_31/products/bios_6_42_03_35/packages;C:/ti/tirtos_tivac_2_14_04_31/products/ndk_2_24_03_35/packages;C:/ti/tirtos_tivac_2_14_04_31/products/uia_2_00_02_39/packages;C:/ti/ccsv6/ccs_base;" xdc.tools.configuro -o configPkg -t ti.targets.arm.elf.M4F -p ti.platforms.tiva:TM4C1294NCPDT -r release -c "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5" --compileOptions "-mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path=\"C:/Users/Vaggelou/Desktop/A R T/ART16/~~~ARTlogger~~~/vaggelou_workspace/gpiointerrupt_EK_TM4C1294XL_TI_TivaTM4C1294NCPDT\" --include_path=\"C:/ti/tirtos_tivac_2_14_04_31/products/TivaWare_C_Series-2.1.1.71b\" --include_path=\"C:/ti/tirtos_tivac_2_14_04_31/packages/ti/drivers/wifi/cc3100/Simplelink\" --include_path=\"C:/ti/tirtos_tivac_2_14_04_31/packages/ti/drivers/wifi/cc3100/Simplelink/Include\" --include_path=\"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/include\" -g --gcc --define=ccs=\"ccs\" --define=PART_TM4C1294NCPDT --define=ccs --define=TIVAWARE --diag_wrap=off --diag_warning=225 --diag_warning=255 --display_error_number --gen_func_subsections=on " "../gpiointerrupt.cfg"
making package.mak (because of package.bld) ...
generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ...
configuring gpiointerrupt.xem4f from package/cfg/gpiointerrupt_pem4f.cfg ...
generating custom ti.sysbios library makefile ...
Starting build of library sources ...
making C:/Users/Vaggelou/Desktop/ART~1/ART16/~~~ARTlogger~~~/vaggelou_workspace/gpiointerrupt_EK_TM4C1294XL_TI_TivaTM4C1294NCPDT/src/sysbios/sysbios.aem4f ...
gmake[1]: Entering directory `C:/Users/Vaggelou/Desktop/ART~1/ART16/~~~ARTlogger~~~/vaggelou_workspace/gpiointerrupt_EK_TM4C1294XL_TI_TivaTM4C1294NCPDT/src/sysbios'
clem4f C:/ti/tirtos_tivac_2_14_04_31/products/bios_6_42_03_35/packages/ti/sysbios/BIOS.c ...
C:/Users/Vaggelou/AppData/Local/Temp/make23936-1.sh: 1: Syntax error: Unterminated quoted string
gmake[1]: *** [BIOS.obj] Error 2
gmake[1]: Leaving directory `C:/Users/Vaggelou/Desktop/ART~1/ART16/~~~ARTlogger~~~/vaggelou_workspace/gpiointerrupt_EK_TM4C1294XL_TI_TivaTM4C1294NCPDT/src/sysbios'
gmake: *** [C:/Users/Vaggelou/Desktop/ART~1/ART16/~~~ARTlogger~~~/vaggelou_workspace/gpiointerrupt_EK_TM4C1294XL_TI_TivaTM4C1294NCPDT/src/sysbios/sysbios.aem4f] Error 2
Build of libraries failed.
error: xdc.cfg.SourceDir: "C:/ti/xdctools_3_31_01_33_core/packages/xdc/cfg/SourceDir.xs", line 209: xdc.cfg.SourceDir : Build of generated source libraries failed: exit status = 2:
js: "C:/ti/xdctools_3_31_01_33_core/packages/xdc/cfg/Main.xs", line 160: Error: Configuration failed!
gmake.exe: *** [package/cfg/gpiointerrupt_pem4f.xdl] Error 1
gmake.exe: *** Deleting file `package/cfg/gpiointerrupt_pem4f.xdl'
gmake.exe: *** [package/cfg/gpiointerrupt_pem4f.xdl] Deleting file `package/cfg/gpiointerrupt_pem4f.h'
gmake.exe: *** [package/cfg/gpiointerrupt_pem4f.xdl] Deleting file `package/cfg/gpiointerrupt_pem4f.c'
js: "C:/ti/xdctools_3_31_01_33_core/packages/xdc/tools/Cmdr.xs", line 51: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
gmake: Target `all' not remade because of errors.
**** Build Finished ****
If I get this right, there might be some files that the CCS can't find or something like that?
Any help is apprieciated. Thanks in advance for the answers.