I have installed ccsv6.1.3 on Ubuntu 14.04 x86 64bit.
I used the TI app store to install TI-RTOS for Tiva-C. That installed tirtos_tivac_2_16_01_14 and xdctools_3_32_00_06 (I think I actually have several copies of xdctools)
I used Resource explorer to find the "hello" example and imported the project. The project was created fine.
When I try to build I get an error that indicates that "XDCTOOLS_JAVA_HOME is set, but does not appear to be a directory containing a 64-bit Java Runtime Environment (1.7 or greater): e.g., '/usr/lib/jvm/java-7-openjdk-amd64'. I do see on the console log that it is trying to use xdctools_3_32_00_06_core/xs
I had a similar issue when I was building the examples from the command line. There I had a copy of the examples dir and edited the makedefs file for my system paths and TI ARM compiler version (15.12.1.LTS). In there I defined & exported XDCTOOLS_JAVA_HOME to exactly the path in the error messages as I have that package already installed. I had only copied 4 examples but they built fine this way.
To workaround the CCS issue I tried defining XDCTOOLS_JAVA_HOME in the workspace env settings
(Menu: Window/Preferences, Dialog: General/Code Composer Studio/Build/Environment)
This did not help. I presume that CCS is setting XDCTOOLS_JAVA_HOME to <install>/ti/ccsv6/eclipse/jre which is a 32 bit JRE and xdc needs a 64 bit JRE.
My workaround was to create a symlink named jre in the xdstools directory: (adjust the cd command for your installed location)
$ sudo apt-get update; sudo apt-get install openjdk-7-jre
$ cd ~/ti/xdstools_3_32_00_06_core
$ ln -s /usr/lib/jvm/java-7-openjdk-amd64/jre
Note: a symlink to /usr/lib/jvm/java-7-openjdk-amd64 does not work for some reason even though both paths work fine as settings for XDCTOOLS_JAVA_HOME.
IAR has a similar issue[1]. The second work around there should also work but the symlink is easier.
I know this should get fixed when ccs7 goes to 64 bit but is there a fix planed for the ccsv6 series?
Bill
[1] wiki.tiprocessors.com/.../TI-RTOS_Xdctools_Java_Home_IAR