I have created a project in CCS v3.3. I have given the path in the build options for the .obj files to be kept in the $(Proj_dir)\Debug folder.....
When i am building the project i can see the .obj files in the folder mentioned above. But when it comes to the linking stage it says it cannot find those .obj files... can any one help me in getting over this errors.
And i have a library file with an extension (.a55). In the build options, in linker\ libraries tab i have included the path of the lib file in search path and the name of the file in Incl. Libraries. But it still doesnt include the library file in the project. I dont understand why even after giving the right path and file name it doesnt include the file in the library.
Please help me debugging these errors.
Regards,
Dinesh Davuluru
Signalogic
Attaching the errors for your reference.
<Linking>
"D:\\Dinesh Davuluru\\ADT Software code\\T38 FAX RELAY\\FAX\\systems\\relay\\c5500\\filerelay\\FileRelay.cmd", line 27: error:
cannot find file "buflog.obj"
"D:\\Dinesh Davuluru\\ADT Software code\\T38 FAX RELAY\\FAX\\systems\\relay\\c5500\\filerelay\\FileRelay.cmd", line 51: error:
cannot find file "buflog.obj"
"D:\\Dinesh Davuluru\\ADT Software code\\T38 FAX RELAY\\FAX\\systems\\relay\\c5500\\filerelay\\FileRelay.cmd", line 73: error:
cannot find file "faxmem.obj"