Other Parts Discussed in Thread: BOOSTXL-EDUMKII
Hi, when I copy the example code for the BOOSTXL-EDUMKII Microphone into the CCS Cloud and try to compile it displays fatal error #1965 cannot open source file "msp.h". All of the other example code for devices on the BOOSTXL-EDUMKII works fine it is only the Microphone application that fails to build. It would appear that the project properties may be incorrect but I don't seem to be able to try something different here.