Other Parts Discussed in Thread: UNIFLASH
Hello everyone,
I want to generate a "Standalone command line" to flash a F28M35H52.
I am not able to construct a "mutlicore" "Standalone folder" in order to flash both core at the same time.
What I do :
- New session
- Select F28M35H52 proc
- Select XDS100 v2 probe
- I select a program (.out from CCS) in Progam/Cortex_M3
- I select a program (.out from CCS) in Progam/C28xx_0
- In the "Standalone Command Line" menu, in the "Images" field, only 1 images is described. NOK
- If I look into the generated folder, only the ARM image has been embedded. NOK
Is it possible to create such standalone folder to flash everything at the same time ?
Is it a bug in the Uniflash v4 ? ( by the way I using the version Uniflash "local" 4.0.974)
Many thanks for your answer,
Thomas