This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Segger J-Link support appears to be incomplete in CCS 7.0.0.00022

The Code Composer Studio v7.0 Release Candidate Wiki entry says:

SEGGER J-Link support integrated in CCS

When using CCS 7.0.0.00022 with SEGGER J-Link 6.10.0.g and SEGGER J-Link USB Driver 1.0.0.6 under Windows 7 can start a debug session for a MSP432 device and step using a Segger J-Link. However, there is some functionality missing in that:

1) If attempt to use the Hardware Trace Analyzer, for the Statistical Function Profiling or Interrupt Profiling, get the following error:

2) Under the CCS Breakpoints there is only a "Breakpoint" option, i.e. no ability to set Watchpoints:

Is it planned to add Hardware Trace Analyzer and Watchpoint support for the Segger J-Link under CCS 7?