This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS 7.0.0.00033 crashes when attempt to start Statistical Function Profiling on a MSP-EXP432P401R

With CCS 7.0.0.00033 under Windows 7 was attempting to use Statistical Function Profiling to debug a program on a MSP-EXP432P401R which was suffering a Usage Fault before reaching main. The XDS110 JTAG / SWD / cJTAG mode was was to "SWD - Mode - Aux COM port is target TDO".

After starting a debug session, with the program halted at the reset vector, selected Tools -> Hardware Trace Analyzer -> Statistical Function Profiling and selected Start using the defaults (Transport Type of SWO Trace and Sampling Interval1024 Cycles). On attempting to Start the Statistical Function Profiling CCS crashes with Windows displaying the following:

The crash has occurred on 3 out of 3 attempts.

The crash dump files for the 3 occurrences of the crash are attached. WERE12D.tmp.WERInternalMetadata.zipWER99A1.tmp.WERInternalMetadata.zipWERD53A.tmp.WERInternalMetadata.zip