Other Parts Discussed in Thread: TMS320F28335, , CC3200
Tool/software: Code Composer Studio
Hi. I've got a problem with my CCS5.3 and CCS7. The problem is the same for both versions of CCS.
A week ago I worked with TMS320F28335 using CCS5.3 on my notebook with Windows 7 and all worked well. But at the present time I use another notebook with Windows 10. At first I installed CCS5.3 on it and tried to work with my projects and targets. It worked well as on previous notebook. I hasn't worked with CCS for a couple of days. Then I installed my other soft that I needed and CCS7. Yesterday I wanted to connect to TMS320F28335 and work with it like I did it before but I've got a problem: CCS5.3 always shuts down on debug session with Windows message "program has stopped working". CCS7 behaves same.
I use XDS200/XDS220ISO, the latest XDS Emulation Software Package v6.0.504.2. CCS closes when I try to connect TMS320F28335 via JTAG using either of them.
Settings:
The JTAG-test always ends with success.
I've tried to do what written in chapter "Is the issue happening when starting a debug session?" here (processors.wiki.ti.com/.../Debugging_JTAG_Connectivity_Problems) and found out that I have a problem on connection to target phase and CCS closes itself (or maybe Windows closes it) without any errors description.
I repeat that emulators and target (TMS320F28335) work well. The problem is with CCS or its Windows 10 compatibility. How can I solve it?