Tool/software: Code Composer Studio
I have two fresh installations of Ubuntu 16.04 LTS using VirtualBox. I've installed the CCSv7 and CCSv6.2 on both machines, respectively. I've also installed the latest ti linux sdk on both machines. My goal is to get through the PRU Training content. I don't get very far...
In the toggle_led demo, at the point where I connect to the CortxA8, and after the PRU_CAPE.gel is run, when I try to connect to PRU0, CCS immediately crashes. This is persistent. I've followed some of the other threads here and attempted to delete the .metadata file, but that doesn't work either.
Not sure what the deal is. Really frustrating. These are fresh installations with latest updates installed.