Hello all,
Tools used:
-CCS 4.1.2.00027 (microcontroller license)
-RDK-IDM-SBC with CCS (processor LM3S9B92)
-EKS-LM3S9B92 (evaluation kit). I'm using the ICDI part of the Eval Kit in order to flash and debug software on the RDK.
Problem:
When trying to debug a project through "Debug Active Project" on Code Composer I get the message:
CORTEX_M3_0: GEL Output: Memory Map Initialization Complete CORTEX_M3_0: Error Connecting to the target Invalid Licence type
I tried everything (resetting the board, power cycling, re-starting Code Composer, updating Code Composer, etc., etc.)
I repeat I have a microcontroller licence, after I launch Code Composer it appears as (Licensed) (window title on the top)
I usualy get working the ICDI board with the second board from the Evaluation kit.
At this stage I wonder if I should send back the two boards (the RDK + the Eval Kit).
Regards,
Cristian