Part Number: EK-TM4C1294XL
Other Parts Discussed in Thread: ENERGIA
Tool/software: Code Composer Studio
When debugging a program in EK-TM4C1294XL using CCS 7.1.0.00016 with TI Emulators 6.0.579.0 under Windows 7 wanted to assert a system reset when started a debug session, in order to place the peripherals into their default state, by setting the "Reset the target on a connect" option:
When a debug session is started the target is not reset, as indicated by the peripheral registers not being reset (e.g. LEDs connected to GPIOs stay lit whereas the GPIOs should be tri-stated on a reset).
CCS 7.0.0.00042 with TI Emulators 6.0.579.0 behaves the same as CCS 7.1.0.00016.
Whereas CCS 6.2.0.00050 with TI Emulators 6.0.579.0 does reset the target when starting a debug session with "Reset the target on a connect" selected.
Has there been a change between CCS 6.2.0 and CCS 7.0.0 w.r.t. the handling of the "Reset the target on a connect" option?