This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler: CCS V7 JTAG failure during connection to PRU



Tool/software: TI C/C++ Compiler

Hi,

the CCS7 crashes when I try to make the connection with the PRU (BeagleBone black + XDS100v2). I have installed the CCSV7.1.0 in ubuntu 16.04 LTS, in the ti folder. Before the installation I have uninstalled the previous release and deleting the folder.
If I run the ccs from terminal I obtain these scripts:
dvtLogOptions.xml DOES NOT exists
... free(): invalid pointer ....

My CCS, after every cresh and restart, sends the report by mail...

I executed also the fsclean command, without success.
I create a new workspace and then a new peroject, without success.

What can I do? There is a release that works in Ubunto?
I had this issue also with CCS6.2 and, some month ago, sometimes it worked;  but now it doesn't work anymore. For these reason I deleted all the installation in order to try the CCS7 release, but it crashes allways like the CCS6.

Thanks for your help
Matteo5265.LogFiles.zip