Other Parts Discussed in Thread: CCSTUDIO
Heya'll,
I'm trying to connect CCS V3.3 with my C6713 DSP Processor on Windows 7, but everytime I try to connect it, the following error comes up.
----------------------------------------------------------------
I/O Port = 540
Board Name: C6713 DSK
Cpu Name: CPU_1
Abort: Close Code Composer Studio.
Retry: Try to initialize the emulator again.
Ignore: Ignore the initialization error and start
potentially without target debugging access.
Diagnostic: Run diagnostic utility.
----------------------------------------------------------------
when I ignore it, it just won't connect to the DSP Processor.
when I click on Diagnostic following dialog box appears:
----------------------------------------------------------------
Diagnostic Utility: "" failed to load
----------------------------------------------------------------
what should I do now?