This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TM4C129XKCZAD: J-link debugger error ""CORTEX_M4_0: Error: Stat [ JLINKARM_IsHalted() call ] failed!""

Part Number: TM4C129XKCZAD

Tool/software: Code Composer Studio

Hi,
I use Code Composer Studio
Version: 7.1.0.00016
MicroController - TM4C129 (Tiva series)
J-Link Ultra+ - debugger

While running development codes for uC I observe code to crash as some points displaying error. What could be the reason for this

""CORTEX_M4_0: Error: Stat [ JLINKARM_IsHalted() call ] failed!""
How to avoid this issue??
even if error appears if I further run the code it runs as expected.Please let me know how to resolve this issue.....

  • Hi,

    The function you mention is the attempt of the Jlink to verify if the target is halted - this is necessary to access the target for any operation (read memory, a register, set a breakpoint, etc.). In this case, I suspect a view may be triggering this - can you close the views opened (variables, registers, memory Browser, etc.) and see which one may cause this message to disappear.

    That is also valid if you are trying to modify something while the target is running - you may get these issues triggered as well.

    I couldn't get this issue here - I tested my Jlink (not Ultra+) with both CCSv7.1.0 and Segger support version 6.10.0n/1.0.0.6 and CCSv7.3.0RC1 and Segger support 6.14.0e/1.0.0.6.

    Hope this helps,
    Rafael
  • Hi
    I tried closing all views .... I still face the issue
    I observe the problem occurs when CCS executes the first instruction
    ui32SysClock = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
    SYSCTL_OSC_MAIN | SYSCTL_USE_PLL |
    SYSCTL_CFG_VCO_480), 120000000);

    If i step thru this portion then it run it then it seems ok....
    Also after building first time if i run the code then too I do not see this issue after closing the view!!
  • Hi,

    Thanks for sending the details; I have seen similar scenarios caused by the change in the PLL that cause an intermediate glitch on the JTAG TCLK frequency - this can trigger the warning message, although I haven't seen this happen with my Jlink yet.

    In the case of XDS Debug probes, I have seen warnings be triggered during these transitions but very randomly. In the cases I observed, there was nothing that could be done. 

    I will try to reproduce this on my Launchpad with code that performs these PLL transitions. 

    Regards,

    Rafael