Tool/software: Code Composer Studio
I am having issues connecting to the Sitara AM3358 on a Rev C Beaglebone Black development board. I'm using CCS 7 and an XDS110 Debug Probe. I am able to connect fine when using my Rev B Beaglebone Black, but when I attempt to connect with a Rev C, I get the following error:
CortxA8: Error connecting to the target: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 7.0.100.0)
I have reviewed multiple threads on e2e with similar issues people have experienced. I am digging through the GEL file to see if there is anything which needs to be tweaked due to any changes between the boards.
Can you provide me details as to exactly what Error -1170 means? Without additional information about the error, establishing root cause and thus a solution is proving very, very time consuming.
Regards,
- Tim Cleveland