Tool/software: Code Composer Studio
When I edit my project properties, like to go back and forth between a control card and my prototype hardware, CCSv7 keeps inserting the linker command file, which I then have to delete per the instructions from my quick guide for setting up a project. If I don't remove it, I have memory overlap errors in the linker. Is there a way to disable this? It is annoying to forget and have all the errors come back, then go back into the project properties, linker file search path and remove the linker command file that it is adding for me automatically. Thanks!