Part Number: TM4C1237H6PZ
Tool/software: Code Composer Studio
Hi Support,
I have a problem with the completion in the header files of a C/C++ project in Code Composer Studio
Basically, completions are available in .c or .cpp files, but do not work in the associated .h files. As additional info, (for #include only) in the header file .h, only the files present in its same folder seems to be listed by the indexer.
Here below an example of what I mean:
- in the test.c file, hitting CTRL+SPACE a list of completions appears
- in the test.h file, hitting the CTRL+SPACE the completions do not appear and "No completions available" is visible in the bottom left corner.
How can I have completions available in the headers files too?
I am running Code Composer Studio Version: 7.2.0.00013, and test is a newly created project for the TM4C1237H6PZ in a newly created workspace
The same seems to happen to my collegues operating with the Code Composer Studio
The same seems not to happen in eclipse Photon 4.8.0M6
Notes:
- I already searched the forums for Code Composer Studio and eclipse
- I already tried all that I could in the indexer and completions options of the Code Composer Studio, but had no success
- this issue seems very similar to mine: https://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/387376/1373367
- I believe it is me missing something as I cannot believe this issue would have not been raised by other users before.
Thanks for your help
Regards,
Alberto