Other Parts Discussed in Thread: UNIFLASH, CC3120
Tool/software: Code Composer Studio
Can not connect to the CC3220 launchpad using Uniflash 422
I have two CC3220 launchpads and neither one will talk to Uniflash422. Both will now allow a download from CCSv8 Debug now that the jumper is removed for SOP (SOP = 000) and a jumper has been added to BRD header thanks to Seong.
I have followed the instructions in the OOB (SWRU473) p32 and run into problems. If I follow their directions and select CC3120/CC3220, Uniflash says that is not supported, and refers me to Uniflashv3. But Uniflash v341 does not support CC3120/CC3220 ????
If I use Uniflash v422 and select CC3220, I can not connect?? I get a timeout error, see below.