Part Number: AM3358
Other Parts Discussed in Thread: AM3359
The pod on the mentioned lauch pad can be isolated from the MSP432 to be used with another target. The BBB has a cTI 20-pin header ( to be populated) and this can be adapted to an ARM 20-pin JTAG header.
Is there a schematic showing how to connect the 10-pin Cortex-M JTag on the launchpad to a standard 20-pin ARM ?
From the BBB ref manual I would infer that the JTAG I/O pins are 3.3 V compatible and can therefore be directly connected to the pod on launchpad . Is this correct ?
Thanks and regards
Peter