Part Number: TM4C129ENCPDT
Tool/software: Code Composer Studio
Working with CCS 8.0.0.00016 on macOS 10.13.3, using the Memory Browser to trace a Fault, and suddenly the display is clipping the last digit of 32-Bit Hex values, both TI Style and C Style, as well as 16-Bit C Style. I have used this feature before on a couple of computers and there were no display problems like this. I cannot find any setting to affect the font size. Resizing the Memory Browser just changes the number of columns, but the last digit in each column is always clipped. I've tried quitting CCS and restarting; I've tried closing the Memory Browser and adding it again; nothing seems to fix this.
I suppose it's possible that the multiple times I've used the Memory Browser were all under macOS Yosemite, but I feel like I've used the Memory Browser at least once on macOS 10.13.3 without this issue. Anyone have an idea of how to fix this? I can view in 64-Bit without clipped digits, but then I have to mentally reverse the order of the 32-bit values.