Tool/software: Code Composer Studio
after connecting CCSV5 and configuring i get this msg but target dont connect
Error connecting to the target:
(Error -151 @ 0x0)
One of the FTDI driver functions used during
the connect returned bad status or an error.
The cause may one or more of: invalid emulator serial number,
blank emulator EEPROM, missing FTDI drivers, faulty USB cable.
Use the xds100serial command-line utility in the 'common/uscif'
folder to verify the emulator can be located.
(Emulation package 5.1.232.0)