Part Number: MSP430FR6989
Other Parts Discussed in Thread: MSP-EXP430FR6989
Tool/software: Code Composer Studio
Hi TI community,
I have an MSP430FR6989 uc, programming it using MSP-EXP430FR6989 launch pad, and I am using CCS 6.1.0
am doing a simple code, where I create an odometer that counts from 0 to 99,999, and then resets again.
This is my code.
#include <msp430.h>
#define DEVELOPMENT 0x5A80
#define ENABLE_PINS 0xFFFE
int main(void)
{
WDTCTL = DEVELOPMENT;
PM5CTL0 = ENABLE_PINS;//this is needed in order to enable pins
P1DIR = 0x01;
P1OUT = 0x00;
unsigned int ones, tens, hund, thou, tnth;
unsigned long km = 0;
while(1)
{
for(tnth = 0;tnth<10;tnth++)
{
for(thou = 0;thou<10;thou++)
{
for(hund = 0;hund<10;hund++)
{
for(tens = 0;tens<10;tens++)
{
for(ones = 0; ones<10;ones++)
{
km = 10000*tnth+1000*thou+100*hund+10*tens+ones;
}
}
}
}
}
P1OUT = ~P1OUT;
km = 0;
}
return 0;
}
I added a breakpoint at P1OUT = ~P1OUT , and pressed the Resume button. (Line 41)

At that line, I see the values of tnth , thou , hund , tens , and ones are equal to 10 , which is as expected.
But I also expected km = 99999 , but instead I got km = 34463 . Shouldn't km = 99999.
Also
I modified my code, and changed thnth , thou , hund , tens , and ones to signed int instead of unsigned int
when I Run my program, and it reaches the breakpoint, I see km > 4,000,000,000

Which doesn't make sense.
I believe the problem is with CCS. I searched online, and some people mentioned that CCS is not synchronizing with the microcontroller, if that was the case, how can I fix it.
I would appreciate your help.
Regards,
Forat