Other Parts Discussed in Thread: MSP430FG439, CC430F5137
I had a CCS Version 5.1.1.00031 installation in which the MSP430 Code Generation Tools had been upgraded to version 4.1.0. I now realize that this was an incompatible combination when selecting an "eabi (ELF)" output format since:
a) The MSP430 Code Generation Tools generated a .data section
b) The MSP430 linker command files in CCS Version 5.1.1.00031 didn't contain a .data section
As a result of the .data section not being in the linker command files, the linker did report warning #10247-D:
The problem is when the linker reports warning #10247-D it seems "random" into which address space the .data section gets placed. e.g.:**** Build of configuration Debug for project MSP430_long_int ****
C:\ti\ccsv5\utils\bin\gmake -k all
'Building file: ../main.c'
'Invoking: MSP430 Compiler'
"C:/ti/ccsv5/tools/compiler/msp430_4.1.0/bin/cl430" -vmsp --abi=eabi -g --include_path="C:/ti/ccsv5/ccs_base/msp430/include" --include_path="C:/ti/ccsv5/tools/compiler/msp430_4.1.0/include" --define=__MSP430FG439__ --diag_warning=225 --display_error_number --printf_support=full --preproc_with_compile --preproc_dependency="main.pp" "../main.c"
'Finished building: ../main.c'
' '
'Building target: MSP430_long_int.out'
'Invoking: MSP430 Linker'
"C:/ti/ccsv5/tools/compiler/msp430_4.1.0/bin/cl430" -vmsp --abi=eabi -g --define=__MSP430FG439__ --diag_warning=225 --display_error_number --printf_support=full -z --stack_size=80 -m"MSP430_long_int.map" --heap_size=300 -i"C:/ti/ccsv5/ccs_base/msp430/include" -i"C:/ti/ccsv5/tools/compiler/msp430_4.1.0/lib" -i"C:/ti/ccsv5/tools/compiler/msp430_4.1.0/include" --reread_libs --warn_sections --rom_model -o "MSP430_long_int.out" "./main.obj" -l"libc.a" "../lnk_msp430fg439.cmd"
<Linking>
warning #10247-D: creating output section ".data" without a SECTIONS
specification
'Finished building target: MSP430_long_int.out'
' '
**** Build Finished ****
a) With a CC430F5137 the .data section got placed in RAM and the program worked.
b) With a MSP430FG439 the .data section got placed in the PERIPHERALS_16BIT area starting at address 0x100, and this caused a watchdog reset in the __TI_decompress_rle_core RTS start-up code before main was entered. An example linker .map file showing this is attached.
In CCS Version 5.2.0.00069 the MSP430 linker command files have been updated to add the .data section (and others) so the incompatibility has been removed. However, given that if a missing SECTIONS causes the linker to place a section in some "random" address space, should linker warning #10247-D really be an error so highlight the problem?
The comment about #10247-D being an error applies to the tms470 Arm Code Generation Tools as well as the MSP430 Code Generation Tools. Sections missing TMS570LS202x6SFlashLnk.cmd in CCS 5.1 is where a missing section in a linker command file caused the tms470 linker to place the .stack and .sysmem sections in flash.