Hi,
I had a project that compiled perfectly in CCS v5.4 (C2000 compiler 6.1.3).
I just installed CCS v6.1 (6.1.0.00104) with C2000 compiler 6.4.4. Then I imported my old project in the new CCS (I didn't recreate the project manually).
Both projects also uses
When trying to compile, I now have a few files that give me this kind of error:
>> path\my_file.c, line 1283:
INTERNAL ERROR: >>>Register allocation failed:
MyFunction
This may be a serious problem. Please contact customer support with a
description of this problem and a sample of the source files that caused this
INTERNAL ERROR message to appear.
Cannot continue compilation - ABORTING!
>> Compilation failure
I tried to change the optimization level in the compiler settings (from off to 1): the previous files with errors now compiled fine, but a new file is showing an issue.
Did anyone experienced the same kind of troubles during CCS version migration? I can see on the forum a few similar posts, but nothing that helped me directly.
Thanks,
Stephane