Other Parts Discussed in Thread: MSP430FR5969
The TI GNU assembler issues a warning if a nop instruction does not follow an enable of interrupts, eint; According to slau367.pdf the proper place is before the eint.
"Include at least one instruction between the clear of an interrupt enable or
interrupt flag and the EINT instruction. For example: Insert a NOP instruction in
front of the EINT instruction." page 42.
The warning when a nop doesn't follow a dint doesn't correctly describe the reason. It says that it is about changes to the interrupt state when the actual reason is that the following instruction is always executed.